cancel
Showing results for 
Search instead for 
Did you mean: 

Half cycle acces ob F1/F3

Uwe Bonnes
Chief
Posted on October 26, 2015 at 15:56

Hello,

what is Half-cycle access  (FLASH_ACR_HLFCYA) for? It may be used with slow clocks ( < 8 MHz)  and AHB divisior = 1.

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Nesrine M_O
Lead II
Posted on October 26, 2015 at 16:48

Hi bonnes.uwe,

Half cycle configuration is not available in combination with a prescaler on the AHB. The system clock (SYSCLK) should be equal to the HCLK clock. 

This feature can therefore be used only with a low-frequency clock of 8 MHz or less. It can be generated from the HSI or the HSE but not from the PLL.

-Syrine-

Uwe Bonnes
Chief
Posted on October 26, 2015 at 17:26

Dear Syrine,

your response repeats what is written in the reference manuals. But is does not answer what Halfcycle access is good for!

Nesrine M_O
Lead II
Posted on October 26, 2015 at 17:55

Hi bonnes.uwe,

Half Cycle Enable Access, if it is set, it halves the period during the flash signals are driven high to save power consumption.

-Syrine-

waclawek.jan
Super User
Posted on October 26, 2015 at 22:10

Syrine,

Thanks for your answer.

Can this info be added to the relevant RMs, please?

Is the upper bound to using this exactly 8MHz? Can this be clearly stated too?

And can the power saving be quantified, best in the datasheet, please?

Thanks

Jan Waclawek

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.