2021-09-20 11:57 AM
in my program is receive first data that tells me what's the size of the payload i am getting next through UART ,When i use that variable as parameter in the UART functions it doesnt work ,however when i hard code a value say HAL_Uart_Receive(&huart1,buffer,5,...) it does indeed work.
Here is my code
#define Max_Buffer_Size 16384UL
uint8_t buffer[Max_Buffer_Size];
HAL_UART_Receive(&huart1,buffer,1,HAL_MAX_DELAY);
int payload_length =buffer[0];
HAL_UART_Receive(&huart1,buffer,payload_length,HAL_MAX_DELAY);as i said if replace line 6 with this is it works :
HAL_UART_Receive(&huart1,buffer,5,HAL_MAX_DELAY);Thank you for your help.
2021-09-20 11:31 PM
Or just drop Cube/HAL and write your own blocking UART receiver. It's literally 5 lines of code.
JW
2021-09-21 12:50 AM
So, try to blink LED when buffer[0] is equal 5. You probably dont receive what you expected.
2021-09-21 4:07 AM
So I tried to implement my own Receive function like this :
void Serial_Receive(uint8_t* buffer ,uint8_t size){
int i=0 ;
while(i < size ){
while (!(USART1->SR & USART_SR_RXNE));
buffer[i]=USART1->DR;
i++;
}
}When i call it with payload_length as a parameter it blocks exactly like the HAL fucntion
Serial_Receive(buffer2,payload_length);A call with a hard coded value proceeds smoothly and the program continues its execution.
Serial_Receive(buffer2,5);The problem probably lies with payload_length variable and I don't see why honestly.
2021-09-21 4:17 AM
I would use DMA in polling modr. Use a cyclic mode over 16 bytes buffer, that is simpler.... and is non blocking...
2021-09-21 4:32 AM
What exactly does the transmitter transmit? Is it
05 xx xx xx xx
or
05 xx xx xx xx xx
?
JW
2021-09-21 5:37 AM
Okay will try it.
I just want to understand what's the problem in this case tbh.
2021-09-21 5:39 AM
first he transmits 5 and then transmits a 5byte string lets say "Hello".
2021-09-21 5:55 AM
Okay, and what is the result of something like
if (payload_length == 5)
LED_ON();
else
LED_OFF();
?
You should consider using a working environment which enables the nowadays usual debugging facilities (breakpoints, single-stepping, observing memories/variables etc.)
JW
2021-09-21 5:57 AM
Probably payload_length isn't what you think it is. What other explanation could there be? The variable is passed by value. The function itself has no idea if you passed a literal or a variable.
2021-09-21 6:10 AM
Led doesn't turn on payload_length is the problem.Also i test buffer[0] instead of payload_length,LED doesn't turn on.
I am not getting the data i expect i guess ?
Also can't really debug because i use those chinese st-link clone to flash and then and FTDI chip to test the uart communication.Can't have both at the same time.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.