2022-05-23 4:00 AM
I am using the stm32h745 nucleo . I am working with the timers and I am getting the falling capture of the cm7 pulse and going in to the callback function when I am using the HAL_TIM_IC_Start_IT() and also I am able to debug the both cm7 and cm4.
But I am not able to do the same thing While I am using the HAL_TIM_IC_Start_DMA() for finding the falling edge. Even I am not able dbug the cm4 when the cm7 is running.
Anyone could you please suggest me how can I do this.
Thanks
Sm
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.