2017-05-02 6:05 AM
After having sent a buffer to my eeprom using the i2c bus, I wait 20 ms in order to wait till the data are stored in the eeprom.
Can someone suggest me a way to poll the i2c bus to know when all the data are stored?2017-05-02 6:58 AM
Read the datasheet of your undisclosed external EEPROM.
It might have a Busy-Flag in a status register, which tells you if an operation is ongoing. Or the document describes another way detecting the operational status.
2017-05-02 7:41 AM
Usually, while the write is in progress, trying to read data from eeprom will fail as the slave device will nack: You will be reading 0xFF...
Poll every 1 msec trying to read data until it is successful then exit the loop. You'll probably want to check if the writing was successful...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.