2018-02-22 1:16 AM
Hi community,
i got a problem by sending udp packets via HAL_ETH_TransmitFrame() on my STM32F107. Sometimes (every x packets) the function gives HAL_BUSY back. I dont know why and i have no idea how to fix this.
It seems that something is locking the eth handler....
I try to fix this issue since a few days now and would be really happy if anybody can give me a suggestion how to fix this.
Best regards,
Mathias
2018-02-23 3:11 AM
Hi
Zviedris.Mathias.002
,As we don't know so much about your hardware, firmware and configuration, I suggest the following:
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2018-02-23 6:01 AM
Hi Amel,
thank you for your response. Iam on a STM32F107 with already working Webserver (Data on SD-card) and CAN Bus to a STM32F105. It figured out, that the error only occours if i have the following situation:
1. Send data via UDP to STM32F107
2. The STM32F107 is sending the data to the STM32F105 (via CAN-BUS)
3. When the operation on the STM32F105 has finished, the uC sends an echo over CAN-BUS to STM32F107
4. In the CAN-RX callback there is a check if the echo is valid
5. If the echo (from the STM32F105) is valid there is a HAL_ETH_TransmitFrame() call within the callback.
Sometimes it works 1000 times in a row and sometimes there´s a 'HAL_BUSY' what is locking the process so that the HAL_ETH_TransmitFrame() isn't sending anything.
I dont know what is the cause of 'ETH->Lock == HAL_LOCKED' ....
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.