2024-01-19 4:16 AM
hi,
DMA setting is in NORMAL mode
i am getting output GPIO-C Port via tim2_up .
HAL_DMA_Start_IT(&hdma_tim2_up, (uint32_t)pixelclock, (uint32_t)&(GPIOC->ODR), 2);
it's working fine but i need to enable call back once data is transferred .
the following Xfercpltcallback is ""not working "".
void XferCpltCallback(DMA_HandleTypeDef *hdma)
{
flag++;
}
which call back i need to use for DMA data transfer completion
Solved! Go to Solution.
2024-01-19 6:31 AM
Hello @MMARI.1 ,
Can you please share your DMA configuration ?
Here is an extract from the STM32CubeF1 FW under the root STM32Cube_FW_F1_V1.8.0\Projects\STM3210E_EVAL\Examples\DMA\DMA_FLASHToRAM :
static void DMA_Config(void)
{
/*## -1- Enable DMA1 clock #################################################*/
__HAL_RCC_DMA1_CLK_ENABLE();
/*##-2- Select the DMA functional Parameters ###############################*/
DmaHandle.Init.Direction = DMA_MEMORY_TO_MEMORY; /* M2M transfer mode */
DmaHandle.Init.PeriphInc = DMA_PINC_ENABLE; /* Peripheral increment mode Enable */
DmaHandle.Init.MemInc = DMA_MINC_ENABLE; /* Memory increment mode Enable */
DmaHandle.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD; /* Peripheral data alignment : Word */
DmaHandle.Init.MemDataAlignment = DMA_MDATAALIGN_WORD; /* memory data alignment : Word */
DmaHandle.Init.Mode = DMA_NORMAL; /* Normal DMA mode */
DmaHandle.Init.Priority = DMA_PRIORITY_HIGH; /* priority level : high */
/*##-3- Select the DMA instance to be used for the transfer : DMA1_Channel1 #*/
DmaHandle.Instance = DMA_INSTANCE;
/*##-4- Initialize the DMA stream ##########################################*/
if(HAL_DMA_Init(&DmaHandle) != HAL_OK)
{
/* Initialization Error */
Error_Handler();
}
/*##-5- Select Callbacks functions called after Transfer complete and Transfer error */
HAL_DMA_RegisterCallback(&DmaHandle, HAL_DMA_XFER_CPLT_CB_ID, TransferComplete);
HAL_DMA_RegisterCallback(&DmaHandle, HAL_DMA_XFER_ERROR_CB_ID, TransferError);
/*##-6- Configure NVIC for DMA transfer complete/error interrupts ##########*/
/* Set Interrupt Group Priority */
HAL_NVIC_SetPriority(DMA_INSTANCE_IRQ, 0, 0);
/* Enable the DMA STREAM global Interrupt */
HAL_NVIC_EnableIRQ(DMA_INSTANCE_IRQ);
/*##-7- Start the DMA transfer using the interrupt mode ####################*/
/* Configure the source, destination and buffer size DMA fields and Start DMA Channel transfer */
/* Enable All the DMA interrupts */
if (HAL_DMA_Start_IT(&DmaHandle, (uint32_t)&aSRC_Const_Buffer, (uint32_t)&aDST_Buffer, BUFFER_SIZE) != HAL_OK)
{
/* Transfer Error */
Error_Handler();
}
}Have you respected the 7 steps ?
Best Regards,
Pierre
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-01-19 6:31 AM
Hello @MMARI.1 ,
Can you please share your DMA configuration ?
Here is an extract from the STM32CubeF1 FW under the root STM32Cube_FW_F1_V1.8.0\Projects\STM3210E_EVAL\Examples\DMA\DMA_FLASHToRAM :
static void DMA_Config(void)
{
/*## -1- Enable DMA1 clock #################################################*/
__HAL_RCC_DMA1_CLK_ENABLE();
/*##-2- Select the DMA functional Parameters ###############################*/
DmaHandle.Init.Direction = DMA_MEMORY_TO_MEMORY; /* M2M transfer mode */
DmaHandle.Init.PeriphInc = DMA_PINC_ENABLE; /* Peripheral increment mode Enable */
DmaHandle.Init.MemInc = DMA_MINC_ENABLE; /* Memory increment mode Enable */
DmaHandle.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD; /* Peripheral data alignment : Word */
DmaHandle.Init.MemDataAlignment = DMA_MDATAALIGN_WORD; /* memory data alignment : Word */
DmaHandle.Init.Mode = DMA_NORMAL; /* Normal DMA mode */
DmaHandle.Init.Priority = DMA_PRIORITY_HIGH; /* priority level : high */
/*##-3- Select the DMA instance to be used for the transfer : DMA1_Channel1 #*/
DmaHandle.Instance = DMA_INSTANCE;
/*##-4- Initialize the DMA stream ##########################################*/
if(HAL_DMA_Init(&DmaHandle) != HAL_OK)
{
/* Initialization Error */
Error_Handler();
}
/*##-5- Select Callbacks functions called after Transfer complete and Transfer error */
HAL_DMA_RegisterCallback(&DmaHandle, HAL_DMA_XFER_CPLT_CB_ID, TransferComplete);
HAL_DMA_RegisterCallback(&DmaHandle, HAL_DMA_XFER_ERROR_CB_ID, TransferError);
/*##-6- Configure NVIC for DMA transfer complete/error interrupts ##########*/
/* Set Interrupt Group Priority */
HAL_NVIC_SetPriority(DMA_INSTANCE_IRQ, 0, 0);
/* Enable the DMA STREAM global Interrupt */
HAL_NVIC_EnableIRQ(DMA_INSTANCE_IRQ);
/*##-7- Start the DMA transfer using the interrupt mode ####################*/
/* Configure the source, destination and buffer size DMA fields and Start DMA Channel transfer */
/* Enable All the DMA interrupts */
if (HAL_DMA_Start_IT(&DmaHandle, (uint32_t)&aSRC_Const_Buffer, (uint32_t)&aDST_Buffer, BUFFER_SIZE) != HAL_OK)
{
/* Transfer Error */
Error_Handler();
}
}Have you respected the 7 steps ?
Best Regards,
Pierre
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-01-19 6:32 AM
hdma->XferCpltCallback gets called from HAL_DMA_IRQHandler which should be called from within the actual DMA IRQ handler. Are you doing that? It should be in your stm32fxxx_it.c file.
2024-01-19 6:57 PM
DMA configuration Memory to Perpheral
static void MX_DMA_Init(void)
{
/* DMA controller clock enable */
__HAL_RCC_DMA1_CLK_ENABLE();
/* DMA interrupt init */
/* DMA1_Channel2_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA1_Channel2_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(DMA1_Channel2_IRQn);
}
void HAL_TIM_Base_MspInit(TIM_HandleTypeDef* htim_base)
{
if(htim_base->Instance==TIM2)
{
/* USER CODE BEGIN TIM2_MspInit 0 */
/* USER CODE END TIM2_MspInit 0 */
/* Peripheral clock enable */
__HAL_RCC_TIM2_CLK_ENABLE();
/* TIM2 DMA Init */
/* TIM2_UP Init */
hdma_tim2_up.Instance = DMA1_Channel2;
hdma_tim2_up.Init.Direction = DMA_MEMORY_TO_PERIPH;
hdma_tim2_up.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_tim2_up.Init.MemInc = DMA_MINC_ENABLE;
hdma_tim2_up.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD;
hdma_tim2_up.Init.MemDataAlignment = DMA_MDATAALIGN_WORD;
hdma_tim2_up.Init.Mode = DMA_NORMAL;
hdma_tim2_up.Init.Priority = DMA_PRIORITY_LOW;
if (HAL_DMA_Init(&hdma_tim2_up) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(htim_base,hdma[TIM_DMA_ID_UPDATE],hdma_tim2_up);
/* USER CODE BEGIN TIM2_MspInit 1 */
/* USER CODE END TIM2_MspInit 1 */
}
}
2024-01-19 7:00 PM
Now callback is happening via stm32fxxx_it.c ->HAL_DMA_IRQHandler
void DMA1_Channel2_IRQHandler(void)
{
/* USER CODE BEGIN DMA1_Channel2_IRQn 0 */
/* USER CODE END DMA1_Channel2_IRQn 0 */
HAL_DMA_IRQHandler(&hdma_tim2_up);
/* USER CODE BEGIN DMA1_Channel2_IRQn 1 */
flag++;
/* USER CODE END DMA1_Channel2_IRQn 1 */
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.