2018-01-10 8:28 AM
Hi,
we have an issue with HAL when trying to stop and re-start CDC VCP. Board is discoF4. Based on the example USB_Device/CDC_Standalone/Src/main.c the code works fine after reset (DSPD=11, USBD_STATE_CONFIGURED). Once modified the example we try to stop it using: (A)
USBD_Stop(&hUsbDeviceFS);
USBD_DeInit(&hUsbDeviceFS);When re-starting with the same sequence:
USBD_Init(&USBD_Device, &VCP_Desc, 0); USBD_RegisterClass(&USBD_Device, USBD_CDC_CLASS); USBD_CDC_RegisterInterface(&USBD_Device, &USBD_CDC_fops); USBD_Start(&USBD_Device);It enters USBD_STATE_SUSPENDED with DSPD=01 and shows <<unknown device>> (43). We get the same result if we use:
USB_DevDisconnect (USB_OTG_FS);
USB_StopDevice(USB_OTG_FS);
instead of (A) to try to stop CDC VCP. Would be very grateful if anyone could provide guidance on how to properly stop and re-start CDC VCP. Thanks in advance.
Francis
2018-01-18 5:17 AM
__HAL_RCC_USB_OTG_FORCE_RESET() did the trick. Not a nice solution but we did not had the time to fiddle around.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.