2018-09-06 6:48 AM
Hello,
I generated a fresh CubeMX project which has can bus. HAL_CAN_Init() returns HAL_TIMEOUT.
What could be the possible solution ?
/* CAN init function */
static void MX_CAN_Init(void)
{
CAN_FilterConfTypeDef sFilterConfig;
static CanTxMsgTypeDef TxMessage;
static CanRxMsgTypeDef RxMessage;
/*##-1- Configure the CAN peripheral #######################################*/
hcan.Instance = CAN;
hcan.pTxMsg = &TxMessage;
hcan.pRxMsg = &RxMessage;
hcan.Init.TTCM = DISABLE;
hcan.Init.ABOM = DISABLE;
hcan.Init.AWUM = DISABLE;
hcan.Init.NART = DISABLE;
hcan.Init.RFLM = DISABLE;
hcan.Init.TXFP = DISABLE;
hcan.Init.Mode = CAN_MODE_NORMAL;
hcan.Init.SJW = CAN_SJW_1TQ;
hcan.Init.BS1 = CAN_BS1_4TQ;
hcan.Init.BS2 = CAN_BS2_3TQ;
hcan.Init.Prescaler = 48;
if (HAL_CAN_Init(&hcan) != HAL_OK)
{
/* Initialization Error */
Error_Handler();
}
/*##-2- Configure the CAN Filter ###########################################*/
sFilterConfig.FilterNumber = 0;
sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;
sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT;
sFilterConfig.FilterIdHigh = 0x0000;
sFilterConfig.FilterIdLow = 0x0000;
sFilterConfig.FilterMaskIdHigh = 0x0000;
sFilterConfig.FilterMaskIdLow = 0x0000;
sFilterConfig.FilterFIFOAssignment = 0;
sFilterConfig.FilterActivation = ENABLE;
sFilterConfig.BankNumber = 14;
if (HAL_CAN_ConfigFilter(&hcan, &sFilterConfig) != HAL_OK)
{
/* Filter configuration Error */
Error_Handler();
}
/*##-3- Configure Transmission process #####################################*/
hcan.pTxMsg->StdId = 0x321;
hcan.pTxMsg->ExtId = 0x01;
hcan.pTxMsg->RTR = CAN_RTR_DATA;
hcan.pTxMsg->IDE = CAN_ID_STD;
hcan.pTxMsg->DLC = 2;
}
2018-09-06 7:28 AM
I pulled high to the CAN RX pin and HAL_CAN_Init() returns HAL_OK
Now, HAL_CAN_Transmit returns HAL_TIMEOUT
2018-09-06 1:44 PM
if you needed to pull the Rx pin high that implies that you have transceiver.
that implies that you have no other device on the TTLCanBus
and that is why your Tx is timing out, because no slave has signaled the message has been received.
if you check the scope, you will see the Tx pin continuously outputting data, waiting for a slave to accept the packet.
2018-09-07 6:50 AM
When I check the canbus by osilascope, I see nothing. There is no data output at the Tx pin. What could be the problem.
2018-09-07 3:12 PM
ABOM should be enabled,
where is the code that is failing ?
2018-09-08 12:29 PM
ABOM is enabled. However I see no Tx data at the output.
2018-09-08 12:30 PM
I still get "HAL_CAN_Transmit returns HAL_TIMEOUT"
2018-09-08 4:49 PM
2018-09-09 12:37 PM
here you can see my code.
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration----------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USB_DEVICE_Init();
MX_CAN_Init();
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
HAL_CAN_Transmit(&hcan, 10);
HAL_Delay(100);
HAL_GPIO_TogglePin(GPIOB, GPIO_PIN_0);
}
/* USER CODE END 3 */
}
2018-09-10 3:55 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.