2018-06-05 10:41 PM
I have a 32 gb sd card. I have interfaced it with STM32F407 Discovery board with 1 bit SDIO through Cubemx. When i use a formatted SD card i am able to write files into the card. Now, i want to format the card using some API and then write files into he card. I dont want to do the formatting manually. I have come across an API (HAL_SD_ERASE). However, I would like to know what should be the start address and end address of sd card to be used in this API.Are there any examples to use this API?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.