2021-12-15 10:02 PM
I'm using the STM32H725 for development.
An image was displayed on the LCD.
There is only one screen view, and a container is placed under it, and an image is placed in the container.
The image is displayed normally, but the screen is flickering.
However, if I reduce the container size, the screen doesn't break and looks normal.
Please review which settings are strange...
Attach the project and screen video.
2021-12-16 10:34 AM
Read Checking display compatibility considering the memory bandwidth requirements chapter in AN4861.
JW
2021-12-16 3:54 PM
The bandwidth has already been checked, and the sample using the F429 implemented with the same configuration and code is operating normally.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.