2024-04-29 6:48 AM
The STM32 families typically use Quad-SPI for executable external flash, from my research (ref)
But the only H-Series options with Quad-SPI are expensive! Are there any alternative methods to executable external program space?
Solved! Go to Solution.
2024-04-29 9:15 AM
Define "Expensive" for me..
STM32H563 / STM32H573 support OCTO/QUAD SPI memories. In meaningful volumes several of these quote out at $5-6, and Serial NOR Flash perhaps a dollar or two.
I can't believe FMC bused external NOR's would be a cheaper route.
May be you can make a list of features, memory sizes, and pins your application needs..
Why the H5 ?
2024-04-29 9:15 AM
Define "Expensive" for me..
STM32H563 / STM32H573 support OCTO/QUAD SPI memories. In meaningful volumes several of these quote out at $5-6, and Serial NOR Flash perhaps a dollar or two.
I can't believe FMC bused external NOR's would be a cheaper route.
May be you can make a list of features, memory sizes, and pins your application needs..
Why the H5 ?
2024-04-29 9:36 AM
Thank you for the quick response Tesla!! You have given us some meat to chew on, let me dig my teeth in and get back to you
2024-04-29 9:44 AM
So this is an offline conversation, for now we will be in touch next by IM or email. We are considering roadmap flexibility here (e.g. mitigating expanding program sizes, algorithms & such down the road)
Thank you Tesla, in touch next :)!
2024-04-29 9:47 AM
Hi Tesla, drop me a private message or email later when available, we are interested in setting up a call this week to learn more
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.