2015-03-30 7:52 AM
Hello everybody,
My question seems very simple but I would like a definitive answer : Is it possible to group all ports of STM32F407xx and write one data for the new big port? I explain me : I would like to group all ports (A -> I) and write a data of 140 bits. The 16 first bits are written in the port A ... and the 12 last are written in the port I. I don't want to write port by port because it's too long (around 300kHz). I want around 1 MHz and I think it is the only solution. Thanks in advance for your answers or suggestions ! Florian #stm32f407 #port #group2015-03-30 8:17 AM
> Is it possible to group all ports of STM32F407xx and write one data for the new big port?
No. JWWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.