2010-06-01 1:38 AM
Graphic Library firmware
#unavailable-resources #unavailable-resources #setting-a-bad-example #stm322011-05-17 4:53 AM
Oh dear - i have just had the wonderful task of porting the ''ST Graphics Lib'' to another driver/panel combination for one of our customer's.
What can i say - who wrote this code !! Over the years i have used many graphics lib's and i would normally expect a simple driver layer, and usually a 2-3 hour process to add a new basic driver. So far i have been fighting for 2 days and am close to the 'end'. I have got it working now - but what an effort. Please ST can you use a software engineer that understands ''abstraction''. If you are to compete with the offerings from the other vendors then you really need to work on the primitives/driver layer. Cheers Spen2011-05-17 4:53 AM
Hi
Hmm, the last comment is not really motivating to start with... I am searching a practical and free library to display just some text an some pictures on a OLED-display via SPI. --> Is the ST Graphics LIB for this aim a bad choice? --> if yes: can somebody recommend another LIB which is easy to adapt on a ST-Microcontroller? (I also encountered the StellarisWare Graphic LIB which is only royalty free in use with Stellaris microcontrollers...) Spec: - 128x96 pixel - 256 colors - Mircroprocessor: STM32F107, later STM32F20x - OLED-Driver: SSD1351 - Tool: Keil For your help thanx in advance Beat2011-05-17 4:53 AM
Hi Neil
Sorry, I dont understand what your link should help? It refers toMeasuring mains power consumption with the STM32x and STPM01...
Cheers2011-05-17 4:53 AM
''I dont understand what your link should help?''
It is another example where ST refer to firmware examples, but those examples are not available for download. To get the firmware example, you have to contact your FAE or distributor and specifically request it.
2011-05-17 4:53 AM
''Oh dear - i have just had the wonderful task of porting the ''ST Graphics Lib'' to another driver/panel combination for one of our customers. What can i say - who wrote this code !!''
I'm afraid I'd have to agree that much of the STM32 ''example'' code is of very poor quality indeed. See:/f951861e
However, If anyone were looking for examples of how not to write source code - especially source code intended to describe & explain products - it's a goldmine!2011-05-17 4:53 AM
Ok, thanx!
What a pity. But what is the alternative (considering my requirements) when the use of the STM32 Graphic Lib is rather not recommendable?2011-05-17 4:53 AM
You've already mentioned the StellarisWare graphics library - any reason why you don't just use that and a Stellaris chip?
From what I've seen, Luminary Micro's sample code is a rare example of how it should be done...2011-05-17 4:53 AM
Changing the Microcontroller is no option. For the actual project there is already too much implemented on a STM32 and also a hardware-redesign makes no sense. Further, our company has no interest to enlarge the microcontroller-sortiment.
I ask Stellaris if there is a way to use their graphical LIB legally. But its (as expected) not in their interest and not possible. So I'm still interested on recommendations for other GUI-LIBs!! Otherwise I willy-nilly have to use the STM32 GUI LIB... Has somebody some valuable advices/informations when using this LIB? Thanx2011-09-24 11:43 AM
Hi all,
I want to create a window (size 800x600) in Visual Screen Designer For Embedded GUI Library (STM32) but created window has a size more or less 600x500.I can set up th position of objects to be whatever I want but how can I see whole window? An solution for that? Thanks, Dominik2011-09-26 1:57 AM
Has somebody some valuable advices/informations when using this LIB?
Don't!We’re moving the ST Community to a new platform to give you a better and more reliable community experience.