2017-09-08 6:55 AM
Hi,
Now I'm currently working with GPIO control.
And I have an issue to control GPIO,
I came across there's not toggling when I use delay()
For example,
# GPIO toggling not working case
void delay(void){ volatile int i; for(i=0; i<10000000; i++);}while (1) { GPIOG->BSRRL = GPIO_Pin_14; delay(); GPIOG->BSRRH = GPIO_Pin_14; delay();GPIOG->BSRRL = GPIO_Pin_15;
GPIOG->BSRRH = GPIO_Pin_15;GPIO_SetBits(GPIOG, GPIO_Pin_15);
GPIO_ResetBits(GPIOG, GPIO_Pin_15);}
# GPIO toggling working good case
void delay(void){ volatile int i; for(i=0; i<10000000; i++);}while (1){GPIOG->BSRRL = GPIO_Pin_14;GPIOG->BSRRH = GPIO_Pin_14;GPIOG->BSRRL = GPIO_Pin_15;
GPIOG->BSRRH = GPIO_Pin_15;GPIO_SetBits(GPIOG, GPIO_Pin_15);
GPIO_ResetBits(GPIOG, GPIO_Pin_15);}
Could you please let me know what does difference between them?
Why doesn't it toggling whithin delay() ?
2017-09-08 8:55 AM
If you are single stepping it might take a while. The delay might need to be tuned depending on how fast things are running, I chose a million to make sure the on/off would be human perceivable a dozens of MHz. Banging the lines up/down at a MHz is going to be imperceivable to the human eye.
Consider keeping your adventure in one thread, there's no value to having dozens of threads about materially the same evolution of what you're doing.
2017-09-08 9:12 AM
Hi!
The '# GPIO toggling working good case' not includes any delay.
Which way you use to observe the toggling? Do you have an oscilloscope?
Try to give a delay 10 times bigger and use this code.
while (1)
{ GPIOG->BSRRL = GPIO_Pin_14; delay(); GPIOG->BSRRH = GPIO_Pin_14; delay();}
supposed that GPIOG pin 14 is initialized in pushpull output mode.(additionaly in your posted cases in maximum speed.)
Regards
vf
2017-09-08 11:13 AM
I can't understand what you are saying. Could you please let me know more clarify?
2017-09-08 11:16 AM
Yes, I've observed it in oscilloscope.
and I've tested with 10times.
while (1)
{GPIOG->BSRRL = GPIO_Pin_14;delay();GPIOG->BSRRH = GPIO_Pin_14;delay();}
GPIOG->BSRRL = GPIO_Pin_15; GPIOG->BSRRH = GPIO_Pin_15;GPIO_SetBits(GPIOG, GPIO_Pin_15);
GPIO_ResetBits(GPIOG, GPIO_Pin_15);That's working as my expectation, it still does not work with delay().
But If I remove delay() in there, then that's working as good, I can check with oscilloscope..
What kind of things should I have to consider to use GPIO toggling in maximum frequency (speed)?
2017-09-08 11:52 AM
Did you ever measured this delay? Is it too big? put a very small delay and observe in your oscilloscope.
2017-09-08 12:06 PM
Let me check to figure out with small delay.
BTW, I can't understand this, why does delay() affect to another gpio function?
2017-09-08 1:19 PM
The delay slows it down so you can physically see it blink. Oscilloscope not going to be helpful at 0.1 Hz
2017-09-08 1:23 PM
Don't know, you're not very good at explaining the context clearly. Slow signals will be visible to the eye, but difficult to see/sync on a scope.
Make the delay loop smaller, I pulled a million out of the air, try 100 or 1000
In the UK or South/North Korea?
2017-09-09 12:16 AM
I found it from oscilloscope that toggling signal.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.