2015-11-18 9:55 AM
Overview ARM family and FPU type The Hello World Cortex-M C/C++ Project wizard The STM32F7xx C/C++ Project wizard More info
The
https://github.com/gnuarmeclipse
includes a set of open source Eclipse plug-ins and tools to create/build/debug/manage ARM (32-bits) and AArch64 (64-bits) applications and static/shared libraries, using the latest GNU ARM GCC toolchains. Overview ARM family and FPU type The Hello World Cortex-M C/C++ Project wizard The STM32F7xx C/C++ Project wizard More infoStarting with GNU ARM Eclipse version 2.10.2, from November 2015, full Cortex-M7 support was added to the
C/C++ Build→
Settings→
Tool Settingspage; it is now possible not only to select the
ARM family:
cortex-m7, but also to select the new specific
FPU type:
http://gnuarmeclipse.github.io/assets/images/2015/properties-c-settings-tools-family-m7.png
Overview ARM family and FPU type The Hello World Cortex-M C/C++ Project wizard The STM32F7xx C/C++ Project wizard More info
The project wizard was updated to create generic Cortex-M7 projects.
http://gnuarmeclipse.github.io/assets/images/2015/wizard-cortexm-core.png
Overview ARM family and FPU type The Hello World Cortex-M C/C++ Project wizard The STM32F7xx C/C++ Project wizard More infoAnd last, but probably the most useful, a new template to create STM32F7 projects was added.
http://gnuarmeclipse.github.io/assets/images/2015/wizard-stm32f7.png
The wizard currently supports STM32F745xx, STM32F746xx, STM32F756xx, and can create blinky projects for the STM32F746_EVAL and STM32F746_DISCOVERY boards.
The created projects not only pass the build, but are ready to run on the selected boards.
Overview ARM family and FPU type The Hello World Cortex-M C/C++ Project wizard The STM32F7xx C/C++ Project wizard More infoFor more details about the GNU ARM Eclipse project, please refer to the project site
.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.