2017-05-26 7:09 PM
Is there anything I am missing while trying to get my STM32F777 chip into DFU mode?
I have a 25 MHZ OSC (HSE), NRST is pulled high with a 10K resister and BOOT0(pin138) is pulled low with a switch to pull it high on reset/power on.
The chip is totally blank never been programmed, do I need to set any of the option bits or are the defaults correct?
How does the chip detect that USB has been connected; the VBUS pin, the ID pin, or just USB communication?
I would appreciate any help, thanks,
Sheldon
Solved! Go to Solution.
2017-06-05 8:02 PM
So it was a USB impedance problem. thanks for the help
2017-06-05 8:02 PM
So it was a USB impedance problem. thanks for the help
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.