2024-09-13 2:51 AM - last edited on 2024-09-13 2:58 AM by mƎALLEm
Hello,
I want to generate 2 pwm signals, where pwm2 should have a delay from pwm1 (delay should be modified on the fly).
I would also like to know if this operation can be done in HRTIM or other Timers.
Thanks and regards,
Pradeepa P
2024-09-16 2:43 AM - edited 2024-09-16 2:43 AM
Hello @Pradeepa_Pugalenthi ,
You can generate two PWM signals where the second PWM signal has a delay from the first, and this can be achieved using both HRTIM and other advanced-control timers.
You can find the HRTIM configuration and examples in this application note AN4539 (start from section: 2.2 Generating multiple PWMs).
Combined PWM mode details for general-purpose and advanced-control timers are available in the RM0433 (38.3.13 Combined PWM mode).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.