2009-08-18 11:31 AM
FSMC and GPIO Pins-
2011-05-17 4:20 AM
When the FSMC is configured, it uses up to 25 GPIOs for its address bus. There does not appear to be any special configuration techniques to use these GPIOs except that I have set them to be outputs.
My problem, I would like to use a few of these unused address lines for inputs. If I set some of the address line GPIOs to ''input mode'', will the FSMC ignore them as address outputs?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.