2017-01-16 1:17 AM
Hello,
I have added an audio task to the stm32f746g discovery project netconn udp echo server (Freertos + lwip ).
The audio task is very simple.I capture the audio data from the microphone and i play it back.
The audio code works in stand alone mode (without using freertos) but when i use freertos the audio task and the ethernet tasks freeze .The audio is correctly processed ( audio in from microphone is played out without problem ) but the LED1 stop to toggle ( LED1 toggle in audio task ) and all ethernet tasks don't work anymore.
Here is my code of the audio task :
static void my_audio_thread(void *arg)
{
audioBuffer = (uint16_t *)malloc(MIC_SAMPLES * 2);
/* Init OnboardMIC */
BSP_AUDIO_IN_OUT_Init(INPUT_DEVICE_DIGITAL_MICROPHONE_2, OUTPUT_DEVICE_HEADPHONE, 100, DEFAULT_AUDIO_IN_FREQ);
BSP_AUDIO_IN_Record(audioBuffer, MIC_SAMPLES*2);
/* Update the Audio frame slot configuration to match the PCM standard instead of TDM */
BSP_AUDIO_OUT_SetAudioFrameSlot(CODEC_AUDIOFRAME_SLOT_02); /* ATT: size to play in bytes ! */ BSP_AUDIO_OUT_Play(audioBuffer, MIC_SAMPLES*2 * sizeof(uint16_t));for(;;)
{
BSP_LED_Toggle(LED1);
vTaskDelay( 500 ); }}
if i remove the line BSP_AUDIO_OUT_Play(audioBuffer, MIC_SAMPLES*2 * sizeof(uint16_t));
the others tasks are not stopped and LED1 toggle.
If someone could help me to find out the way to resolve this issue it would be great!!!
Thank you.
Félix.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.