2016-08-02 9:05 AM
Please add GNU ARM Eclipse, with a reference to http://gnuarmeclipse.github.io, to the list of free, open source, development environments with strong support for STM32 devices.
Regards,Liviu #free-development-ide-gnu-arm2016-08-13 2:27 AM
any moderator reading this post?
2016-08-15 8:36 AM
Hi Liviu Ionescu,
Thanks for your contribution in the STM32 forum. Do you mean to add GNU ARM Eclipse in the sticky discussion available in this forum?I will check what can be done, if possible please provide more details on the supported devices...-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2016-08-26 12:37 AM
> Do you mean to add GNU ARM Eclipse in the sticky discussion available in this forum?
yes, Mayla, please add the following:* GNU ARM Eclipse (http://gnuarmeclipse.github.io) - supportsall STM32 devices based on ARM Cortex-M0, M0+, M3, M4, and M7 cores. Runs on Windows, GNU/Linux and macOS. Advanced debugging features, including emulator. Completely free, completely open source.
Thank you,Liviu2016-09-07 11:18 PM
Mayla? did you see this message?
2016-10-03 3:05 PM
Mayla? Anyone else moderating this forum?
2016-10-05 1:52 AM
I think that no one should ignore the wonderful work by Liviu Ionescu for the GNU ARM developers community.
Chapeau2016-10-06 2:25 AM
Thank you, @ferri.marcello.
Can anyone help me contact the moderators?Liviu2016-10-06 4:24 AM
There is this ''Contact moderator'' menu there:
2016-10-10 9:40 AM
> There is this ''Contact moderator'' menu
I did this, twice, but it was of no use. :(any other suggestions?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.