2023-12-17 8:08 AM
In the RM it says the above, but the only information i can find in the chapter that is referenced to is: "force boot from FLASH".
Is there a way to define a "unique" entry point, or ist this just wrong in the manual?
2023-12-17 8:25 AM
Perhaps it could be written better, but 0x08000000 is a unique entry point. You cannot boot to an arbitrary FLASH address on this chip. Some families such as the STM32H7 let you put a custom address to boot from.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.