2024-04-22 3:44 PM
Hi,
when I write 8byte block sequentially 256 times in 2kB page and then erase and start over what is the total number of writes I can do?
Datasheet describes 10000 write/erase cycles, but I do not erase after every write.
If the damage is cause by erase should the flash last longer with 1 erase per 256 writes?
can I write 256 times before erase is necessary or it would somehow degrade other cells sooner?
if there is a formula for write/erase damage ratio what is it?
I use stm32g071 but I expect this to be common use case.
Solved! Go to Solution.
2024-04-23 3:22 AM
take a look at this recent thread on the topic:
https://community.st.com/t5/stm32-mcus-embedded-software/issues-with-x-cube-eeprom/m-p/662768#M46987
TL;DR: It's the Erase that causes the wear - not writing.
@PR.10 wrote:I use stm32g071 but I expect this to be common use case.
Yes, it's a common property of all electrically-erasable PROM - not specific to STM32 or even to ST.
2024-04-22 4:12 PM
> should the flash last longer with 1 erase per 256 writes?
> can I write 256 times before erase is necessary
Yes and yes.
2024-04-23 2:51 AM
256x sound great, but it still does not explicitly defines the write limit:
if write is the problem it would be still about 10256
if they are equal it would be about 20000
if only erase is the problem it would up to 2550000
what is close to the reality for the internal flash?
2024-04-23 3:22 AM
take a look at this recent thread on the topic:
https://community.st.com/t5/stm32-mcus-embedded-software/issues-with-x-cube-eeprom/m-p/662768#M46987
TL;DR: It's the Erase that causes the wear - not writing.
@PR.10 wrote:I use stm32g071 but I expect this to be common use case.
Yes, it's a common property of all electrically-erasable PROM - not specific to STM32 or even to ST.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.