2014-07-29 12:40 PM
Hi,
I am using STM32F103R8T6.I normally perform the in-circuit programming using the STMFlashLoader.exeSometimes I need to erase and program some pages performing an In-Application programming. I use the library function FLASH_ProgramWord().The flash gets programmed correctly, but when later on I try to re-program using the STMFlashLoader.exe (I selectively erase only the pages that I program) it gives me error in verifying (''some pages might be write protected'').In order to solve the problem I am obliged to perform an Erase All.Can someone help me on this? Do I miss something?Thanks,Marco #!psychic #flash #stm32l2014-07-29 1:40 PM
Can someone help me on this? Do I miss something?
Seem to be aggravating something. Do you modify the Option Bytes? Can you present a complete/concise example of what you're doing now so I don't have to guess what's going on.2014-07-30 3:39 AM
In the following the function I use to program.
void UserFlashProgram(){ u32 StartUserAdd; u32 EndUserAdd; u32 EraseCounter, Address; vu32 WRPR_Value = 0xFFFFFFFF, ProtectedPages = 0x0; u8 NbrOfPage; u8 IxOfPage; volatile FLASH_Status FLASHStatus; volatile TestStatus MemoryProgramStatus; ErrorStatus HSEStartUpStatus; // Inizializzazione Variabili FLASHStatus = FLASH_COMPLETE; MemoryProgramStatus = PASSED; EraseCounter = 0x0; StartUserAdd = (u32)(0x08000000 + START_FLASH_USER_DATA_ADDRESS); EndUserAdd = StartUserAdd + 0x0400; NbrOfPage = (EndUserAdd - StartUserAdd) / 0x400; IxOfPage = (u32)START_FLASH_USER_DATA_ADDRESS/0x400; // Capire a cosa serve!!!! FLASH_ClearFlag(FLASH_FLAG_BSY | FLASH_FLAG_EOP|FLASH_FLAG_PGERR |FLASH_FLAG_WRPRTERR); // Il WRPR è un registro in cui ogni bit indica se quattro pagine sono Write protected o no WRPR_Value = FLASH_GetWriteProtectionOptionByte(); ProtectedPages = WRPR_Value & (0x00000001 << (IxOfPage/4)); // Pages are write protected if (ProtectedPages == 0x00) { // Disable the write protection FLASHStatus = FLASH_EraseOptionBytes(); // Generate System Reset to load the new option byte values NVIC_GenerateSystemReset(); //////////////////////////////Problema, non restituisco nulla!! } // If Pages are not write protected, perform erase and program operations. Else nothing else { // Clear All pending flags FLASH_ClearFlag(FLASH_FLAG_BSY | FLASH_FLAG_EOP|FLASH_FLAG_PGERR |FLASH_FLAG_WRPRTERR); // Erase the FLASH pages for(EraseCounter = 0; (EraseCounter < NbrOfPage) && (FLASHStatus == FLASH_COMPLETE); EraseCounter++) { FLASHStatus = FLASH_ErasePage(StartUserAdd + (0x400 * EraseCounter)); } Address = StartUserAdd; while((Address < EndUserAdd) && (FLASHStatus == FLASH_COMPLETE)) { // La funzione già di per se mi garantisce che vengano rispettate le attese // C'è un Timeout se non ce la faccio FLASHStatus = FLASH_ProgramWord(Address, AdLp[(Address - StartUserAdd)/4]); Address = Address + 4; } if(FLASHStatus != FLASH_COMPLETE) { SetErrFat(ERR_DATA); return; } // Check the corectness of written data Address = StartUserAdd; while((Address < EndUserAdd) && (MemoryProgramStatus != FAILED)) { if((*(vu32*) Address) != AdLp[(Address - StartUserAdd)/4]) { MemoryProgramStatus = FAILED; } Address += 4; } if(MemoryProgramStatus == FAILED) { SetErrFat(ERR_DATA); return; } }2014-07-30 7:45 AM
The code would seem to have a problem with the Write Protect status if more than one page is being written, you might want to create a mask of all the bits of interest before you do that test.
So, not seeing any code to unlock the flash, change the write protection state, or output any diagnostic information as the flash proceeds. Can your code reflash itself a second time? Does it reset? Is there an issue with the reset? There are a number of defines and variables missing from your example making it difficult to analyze. Can you create a small stand-alone applet, that's compilable, and demonstrates the problem?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.