2014-06-13 11:34 AM
Hi everyone,
I would like to flash programming my Stm3221G-Eval Boards without using The ST_link..I already
configure
the
boot mode
{boot
0,boot1}and the
boards
is properly connected
to the PC
via
an
RS232
cable
...
when I start the
flash
loader
demonstrator
and I
put
the
port's
nameI get
this
error
''verify
the
boot
configuration mode
and the
flash
protection
status''
also i
want to know where
can I get
the binary file
.. thanks.2014-06-13 1:07 PM
The serial channel needs EVEN parity 9600 8E1 should suffice for testing. Also you could used RealTerm, sending an 0x7F hex value, and seeing if a 0x79 is returned.
To generate .BIN files will depend on the tools, FROMELF, OBJCOPY or ELFARM generally would be able to do that, but I seem to recall .HEX files being usable, but that might be for the ST-Link utilities.2014-06-14 4:50 AM
Hi clive1,
Please can you tell me how to load the binary image of the user program to the root directory of a USB key.. Thanks.2014-06-14 5:52 AM
Please can you tell me how to load the binary image of the user program to the root directory of a USB key..
Not sure I completly understand the question, but I'm going to assume you want software that will access a USB Flash Drive and write that to the internal memory of the STM32F2. This example for the STM32F4-Discovery should be reasonably portable STM32F4-Discovery_FW_V1.1.0\Project\FW_upgradeWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.