2016-04-22 10:09 AM
Hi,
I am trying to use the fast program method to write a row (256 bytes) to the flash. But when HAL_Flash_Program() function is called, the PGAERR flag is raised. The input buffer as well as the write address are 256 byte aligned. #flash #stm32l476We’re moving the ST Community to a new platform to give you a better and more reliable community experience.