2017-12-22 1:53 AM
I'm trying to store some data using HAL library.
HAL_FLASH_Unlock();
__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_EOP | FLASH_FLAG_OPERR | FLASH_FLAG_WRPERR | FLASH_FLAG_PGAERR | FLASH_FLAG_PGSERR );
FLASH_Erase_Sector(ADDR_FLASH_SECTOR_10, VOLTAGE_RANGE_3);
uint64_t testVar = 0XFAFAFAFAFAFAFAFA;
HAL_FLASH_Program(TYPEPROGRAM_WORD, ADDR_FLASH_SECTOR_10, testVar);
HAL_FLASH_Lock();
Now
FLASH_Erase_Sector does not erase the sector and that's why I can't program it. Am I missing something?
I tried the same function from STM32F4xx_StdPeriph_Driver library and it works fine. I can see that the two fuctions are different even if they should look the same. Few things I don't understand.
1.In the HAL version of the function FLASH_WaitForLastOperation() is not used.
2.This part is missing
/* if the erase operation is completed, disable the SER Bit */
FLASH->CR &= (~FLASH_CR_SER); FLASH->CR &= SECTOR_MASK;3. This comment seems a bad copy and paste from the
STM32F4xx_StdPeriph_Driver version.
/* if the previous operation is completed, proceed to erase the sector */
4. I can't figure out where this come from, could someone point me to a datasheet?
/* Need to add offset of 4 when sector higher than FLASH_SECTOR_11 */
if(Sector > FLASH_SECTOR_11) { Sector += 4U; }#hal_flash_program-stm32f43 #flash_erase_sector #hal_flash2018-03-18 11:36 PM
I think you're supposed to use HAL_FLASHEx_Erase(FLASH_EraseInitTypeDef *pEraseInit, uint32_t *SectorError) which calls
FLASH_Erase_Sector
internally along with the missing parts from the peripheral library that you have mentioned here.But I'm still having some issue where it is not erased consistently. Sometimes requires multiple calls to successfully erase. Have you had any success with this?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.