2015-09-10 7:06 AM
I have embedded experience with other dev board like TI tiva, NXP's LPC 1769 etc, however, this is my first foray into a STM board. my goal is to port my existing firmware to this board and I'll be glad if someone here can guide me along. So far, I have found STM world to be too complicated software/documentation side compared to other boards I have used; and for whatever reason, I am unable to get any hits using search function on this forum.
I have got the STM32F7-disco, which is my first M7 board, and I have a few questions on how to go about setting it up. I am using the system workbench for STM32 as my IDE since that's the only one I could find which was supported for STM32F7.I am trying to figure out which libraries I'll use for the project; and I am unable to find much options in this regard. I'll like to have as simple a solution as possible. can anyone tell me the starting point for this board? I have ofcourse read through this UM1907:Discovery kit for STM32F7 Series with STM32F746NG MCU, but that doesnt give me a good overview to STM32 tools.
The only other thing I found was UM1905: Description of STM32F7xx HAL drivers; but thats too dense for what I want to do, and I am all ears if I can get away without using HAL.Is this board mbed compatible? can I instead use their libraries for my firmware?2015-09-10 8:51 AM
Hi bigdawg,
Welcome to STM32 world! :)So, STM32F7 discovery kit related documentation is available inhttp://www.st.com/web/catalog/tools/FM116/CL1620/SC959/SS1532/LN1848/PF261641
.This board is mbed compatible; you find the Online IDE for STM32F746G-DISCO at ARM mbed onhttps://developer.mbed.org/platforms/ST-Discovery-F746NG/
(if you have any question on this regard, you can submit it in mbed forum).I am using the system workbench for STM32 as my IDE since that's the only one I could find which was supported for STM32F7. I don't agree with you because these IDEs support already STM32F7: Keil, IAR, SW4STM32.I am trying to figure out which libraries I'll use for the project; and I am unable to find much options in this regard. You have to use the STM32CubeF7 package (http://www.st.com/web/en/catalog/tools/PF261909
) which contains the STM32F7 drivers besides to a set of examples on various use cases based on all peripherals.You can also get initiated withhttp://www.st.com/web/en/catalog/tools/PF259242
: a graphical software configuration tool that allows generating C initialization code using graphical wizards.Hope these inputs will help you to easily start your projects with F7 products.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.