2011-03-21 5:34 AM
FILE AXF
2011-05-17 5:29 AM
If you are unable to use the tools or make this determination, you should probably call Keil technical support and work through it with them.
You should be able to compile/debug directly into the board via JTAG if you have the project/memory set up correctly. The AXF file contains a lot more information beyond the executable code. If you download the AXF directly into the STM32's memory space you might well have a problem as it is not native binary. I wish you'd stick to one thread rather than opening a new one every time you have a thought.2011-05-17 5:29 AM
Hello
Sorry
,
I did not
understand
that
I must do clive1
.
Thank you
Rosa
2011-05-17 5:29 AM
Hello
Since
I
can
not
on
Keil
debugging purposes
must
simulate
directly
on
the target
because
the
maximum file size
for debugging
on
Keil
is
32KB
by
my
file size is941Ko
, you
know
where
the
problem
Thank you
2011-05-17 5:29 AM
''you
know
where
the
problem?''
It seems to me that the problem is that you are trying to run a marathon before learning to crawl - let alone walk. Do you have any prior programming experience in general? Do you have any prior programming experience with small embedded microcontrollers in particular?
Have you taken any time to study the Keil documentation, and familiarise yourself with the tools and their use? Have you taken any time to study the GUI library documentation, examples, etc, and familiarise yourself with the tools and their use?
2011-05-17 5:29 AM
Sounds like you need to get a properly licensed version of Keil to work on an application of that size.
How are you writing the AXF to the part? Can you generate a BIN or HEX file and program that with J-Flash or ST-LINK?2011-05-17 5:29 AM
''... simulate
(sic)directly
on
the target...''
If your're running the actual code on the actual target, then that's not simulating - is it?! That's the Real Thing - not a simulation!
2011-05-17 5:29 AM
Hello neil.andrew
We can
say that
I mastered
the
programming,
graphics
library
,
user
manual
touchscreen
with
this library
I
said
the
simulation
, ie
testing
the
program on
the
target board
Thank you
Rosa
2011-05-17 5:29 AM
''We can say that I mastered the programming, graphics library, user manual touchscreen with this library''
We could say it - but your posts give a very different impression!''I said the simulation, ie testing the program on the target board''
No, that is not simulation.Simulation refers to something that is not the real thing
http://dictionary.cambridge.org/dictionary/british/simulation
2011-05-17 5:29 AM
I did not
understand
''
my
messages
give
a
very
different
impression
''
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.