2020-05-14 5:06 AM
A program, using the Nucleo-64 with STM32L073RZ, gives no problems, another program, even a blank new project, with Nucleo-64 with STM32L476RG gives
"Failed to execute MI command:
target remote localhost:61234
Error message from debugger back end:
Remote communication error. Target disconnected.: Success.
Failed to execute MI command:
target remote localhost:61234"
2020-05-16 8:26 AM
Debugging issues are tightly coupled to the IDE, so posting the one you're using is helpful. Those chips may have different ST-Link versions/capabilities which require different ST-Link configuration files.
2020-05-17 11:59 PM
My apologies. I posted this in a hurry. To much of a hurry I fear :). I am using the ST Microelectronics own STM32CubeIDE version 1.3.0 (build 5720_20200220_153). I have forced the Nucleo-84 on-board ST-Link_V2-1 into an upgrade mode and downloaded version V2J36M26 to see if that cured the issue, unfortunately it didn't.
This is what I get in the console now:
Device ID: 0x415
PC: 0x0
ST-LINK detects target voltage = 3.25 V
ST-LINK device status: UNKNOWN
ST-LINK device initialization OK
Waiting for debugger connection...
Waiting for connection on port 61234...
Accepted connection on port 61234...
Debugger connected
Try halt...
2020-05-18 12:22 AM
This is what I get in the console now:
Device ID: 0x415
PC: 0x0
ST-LINK detects target voltage = 3.25 V
ST-LINK device status: UNKNOWN
ST-LINK device initialization OK
Waiting for debugger connection...
Waiting for connection on port 61234...
Accepted connection on port 61234...
Debugger connected
Try halt...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.