2021-01-10 11:02 AM
I am working with CubeIDE 1.4.0 on Windows 10 and using STM32L151V8T6A on my prototype board.
However not able to fix the errors below.
Would be of great help to get to know and fix the cause
Thanks a lot
Error message from debugger back end:
Error finishing flash operation
Failed to execute MI command:
load C:\\Robertshaw\\Projects\\WHC_BB01\\Debug\\WHC_BB01.elf
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a10532.srec
File : ST-LINK_GDB_server_a10532.srec
Size : 7164 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Error: Flash loader cannot be loaded
Error: failed to erase memory
Encountered Error when opening C:\ST\STM32CubeIDE_1.4.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_1.4.0.202007081208\tools\bin\STM32_Programmer_CLI.exe
Error in STM32CubeProgrammer
Debugger connection lost.
Shutting down...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.