2017-11-23 5:59 PM
On F446RC, sysreset does not put bit 19 into default setting of 0, its stuck on 1 if 1 is written previously.
Procedure to set and clear bit:
RTC->CR = (0<<19); //Clear bit19, 512hz mode
RTC->CR = (1<<19); //Set bit19, 1hz mode2017-11-24 1:14 AM
This is the correct behaviour, as RCC_CR is in the backup domain - read 6.1.3 Backup domain reset and the RCC_CR description in RCC registers chapter.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.