2018-02-02 11:27 PM
I have created a project for stm32f103c8t6 with RTC support and selected 'generate peripheral init as a pair of .c and .h file', toolchain is TrueSTUDIO. It worked nice before the last update. After update to version 4.24 in rtc.c file I see the following mess:
/* Includes ------------------------------------------------------------------*/
&sharpinclude 'rtc.h'&sharpn&sharpn
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
RTC_HandleTypeDef hrtc;
&sharpn/* RTC init function */void MX_RTC_Init(void){&sharptRTC_TimeTypeDef sTime;&sharptRTC_DateTypeDef DateToUpdate;&sharpn&sharpt&sharpt/**Initialize RTC Only &sharpn&sharpt&sharpt*/&sharpthrtc.Instance = RTC;&sharptif(HAL_RTCEx_BKUPRead(&hrtc, RTC_BKP_DR1) != 0x32F2){&sharpthrtc.Init.AsynchPrediv = RTC_AUTO_1_SECOND;&sharpthrtc.Init.OutPut = RTC_OUTPUTSOURCE_NONE;&sharptif (HAL_RTC_Init(&hrtc) != HAL_OK)&sharpt{&sharpt&sharpt_Error_Handler(__FILE__, __LINE__);&sharpt}&sharpn&sharpt&sharpt/**Initialize RTC and set the Time and Date &sharpn&sharpt&sharpt*/&sharptsTime.Hours = 0x1;&sharptsTime.Minutes = 0x0;&sharptsTime.Seconds = 0x0;&sharpn&sharptif (HAL_RTC_SetTime(&hrtc, &sTime, RTC_FORMAT_BCD) != HAL_OK)&sharpt{&sharpt&sharpt_Error_Handler(__FILE__, __LINE__);&sharpt}#rtc-stm32f1xxSolved! Go to Solution.
2018-02-22 8:00 AM
Hello
Sharipov.Almaz
,
This issue will be fixed in the next CubeMX release.
Sorry for any inconvenience it may cause.
BR. Jeanne
2018-02-16 2:51 AM
Hello
Sharipov.Almaz
I confirm this issue and reported it to our CubeMx team for fix.
Thank you for highlighting the issue, and Sorry for any inconvenience it may bring for you.
Best Regards,
Imen
2018-02-22 8:00 AM
Hello
Sharipov.Almaz
,
This issue will be fixed in the next CubeMX release.
Sorry for any inconvenience it may cause.
BR. Jeanne
2018-03-13 6:43 AM
Hello
Sharipov.Almaz
,
Please download the new
with fix of this issue.Best Regards,
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.