2008-08-26 1:21 AM
EXTI Interrupt : how do i know which port has triggerd the ISR?
2011-05-17 3:42 AM
How can i distinguish the source of an interrupt-request for e.g. EXTI0 (PA0, PB0..) in the ISR?
2011-05-17 3:42 AM
on one EXTI-line you can use only one source, it is
selected with the register AFIO_EXTICRx (see http://www.st.com/mcu/forums-cat-7068-23.html). If you use more then one line in the isr (eg. IRQ EXTI9-5) you can use more then one source and you can distinguish the source in the pending register EXTI_PR.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.