2016-06-13 12:37 AM
Hi,
I need help enabling page read mode in external memory .This external memory supports faster asynchronous page reads (shown on page 10) but Ican not find needed information in stm32 if fsmc supports this kind of read operations.Currently I have bottom setup (for default operation): SRAM_Read_Timming.AddressSetupTime = 6; // 0 ~ 15 SRAM_Read_Timming.AddressHoldTime = 1; // 1 ~ 15 SRAM_Read_Timming.DataSetupTime = 6; // 1 ~ 256 SRAM_Read_Timming.BusTurnAroundDuration = 0; // 0 ~ 15 SRAM_Read_Timming.CLKDivision = 2; // 2 ~ 16 SRAM_Read_Timming.DataLatency = 2; // 2 ~ 17 SRAM_Read_Timming.AccessMode = FMC_ACCESS_MODE_A; hsram.Init.NSBank = FMC_NORSRAM_BANK2; hsram.Init.DataAddressMux = FMC_DATA_ADDRESS_MUX_DISABLE; hsram.Init.MemoryType = FMC_MEMORY_TYPE_PSRAM; hsram.Init.MemoryDataWidth = FMC_NORSRAM_MEM_BUS_WIDTH_16; hsram.Init.BurstAccessMode = FMC_BURST_ACCESS_MODE_DISABLE; hsram.Init.WaitSignalPolarity = FMC_WAIT_SIGNAL_POLARITY_LOW; hsram.Init.WaitSignalActive = FMC_WAIT_TIMING_BEFORE_WS; hsram.Init.WriteOperation = FMC_WRITE_OPERATION_ENABLE; hsram.Init.WaitSignal = FMC_WAIT_SIGNAL_DISABLE; hsram.Init.ExtendedMode = FMC_EXTENDED_MODE_DISABLE; hsram.Init.AsynchronousWait = FMC_ASYNCHRONOUS_WAIT_DISABLE; hsram.Init.WriteBurst = FMC_WRITE_BURST_DISABLE; hsram.Init.ContinuousClock = FMC_CONTINUOUS_CLOCK_SYNC_ONLY; hsram.Init.WriteFifo = FMC_WRITE_FIFO_DISABLE; hsram.Init.PageSize = FMC_PAGE_SIZE_NONE;2016-06-13 2:33 AM
No.
JWWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.