2018-05-17 11:19 AM
Hello EE verse,
Can anyone explain the below implementation ?
I did see the reference to this function in the cortex_m4 generic reference manual but couldn't understand how the register is mapped.
Also no sure why in NVIC->ISER, IRQn (6 in my case) will be right shifted by 5? can you explain the logic?
__STATIC_INLINE void __NVIC_EnableIRQ(IRQn_Type IRQn){ if ((int32_t)(IRQn) >= 0) { NVIC->ISER[(((uint32_t)IRQn) >> 5UL)] = (uint32_t)(1UL << (((uint32_t)IRQn) & 0x1FUL)); }}-AM
#interrupts #core_m4 #nvic #nucleo64 #stm32f401re2018-05-17 11:42 AM
The >>5 is DIV32 the & 0x1F is MOD32
The NVIC has an array of 32 bit flags arrayed over multiple words.
IRQ6 with be Bit 6 in Word 0
ISER[IRQ / 32] = 1 << (IRQ % 32); // Write the bit position into the Set/Enable register
ie ISER[0] = 0x00000040;
2018-05-17 1:14 PM
It becomes quite easy to understand once you put the code side by side with the reference manual on the core
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.