2008-01-08 10:31 PM
Exit from Standby Mode
2011-05-17 3:20 AM
Hello,
i would like to know if to wake up the SMT32 from Standby mode, I can configure by software any other pin, apart from Reset, Tamper and WKUP pins (I/O pins are high impedance). I am using a membrane keyboard, that's why I need 2 pins. I have found something on RM0008 (6.2.3. Wakeup event management), but I'm not sure. Thank you.2011-05-17 3:20 AM
It can only be woken up by a rising edge on PA.0 (WKUP pin), but mine does not wake up.
Currently do it like this: ...// Peripheral Clock - This is done in the init function, but I did it again here
RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR,ENABLE); // Enable WKUP pin PWR_WakeUpPinCmd(ENABLE);// Insert a delay - I have also tried without this delay
Delay(0xFFFF); // for(; nCount != 0; nCount--);// Request to enter STANDBY mode and wake up with rising edge of WKUP pin
PWR_EnterSTANDBYMode();while(1)
{ // Infinite loop - It's OK because the system will reset anyways } The unit does not wake up (reset). I've tried with both the JTAG connected and not connected. Port PA.0 (WKUP pin) has a pull-down resistor, leading to a momentary switch, with Vcc on the other side of the switch, which should be enought to generate the required rising edge when the button is pressed. Any ideas?Hello,
i would like to know if to wake up the SMT32 from Standby mode, I can configure by software any other pin, apart from Reset, Tamper and WKUP pins (I/O pins are high impedance). I am using a membrane keyboard, that's why I need 2 pins. I have found something on RM0008 (6.2.3. Wakeup event management), but I'm not sure. Thank you.2011-05-17 3:20 AM
Try not cross posting to 4 threads.
And take a look at STM32F10xFWLib\Examples\PWR\STANDBY\main.c which should be in Keil and IAR tool chains.2011-05-17 3:20 AM
Thank you. And sorry about the cross posting.
GilWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.