2012-10-17 8:36 AM
Hello,
I am new to ST microcontrollers, just maybe 2 weeks ago I accidentally found about this crazy chip (STM32F4) and now i am already playing with it. I am interested in the I2S hardware and audio processing, so i first flashed the audio example. All works fine, then installed Attolic and tried to compile, but off course was not possible. So after lots of reading I have decided to use CooCox IDE. All working and running, just have a problem with converting the Audio Playback example to the CoIDE(MEDIA_IntFLASH configuration). All files are added, dependencies fixed, so when the compiled image is flashed to the board - the green led on start is ok, then the blue is blinking. The pause button works as expected, also the MEMS sensor input is processed all right.But there is no sound on the output. The things i have suspected for the problem and i fixed: - the SystemInit() call missing in the C startup file - done - the correct value of the external cristal changed from 25 Mhz to 8 Mhz - MEDIA_IntFLASH added to defines in the Configuration so relevant parts are compiled It seems next step is to add some debug print and go through init functions, attach the scope, etc. But was just wondering if i am missing something obvious and somebody has been there already and save me from hours debugging. Thank you! BR, Chris2012-10-17 8:51 AM
You probably talking about the stm32f4_discovery board ...
I have never played with the audio chip on this board, but: - First, it's a good idea to get the datasheet of this chip. - Second, I2S is a synchronious bus, you should see clock signals at the according pins. - Third: a scope is really recommended when working with a serial bus. Atollic and Coocox are both Eclipse-based, which might have eased the porting...2012-10-17 9:07 AM
Hi fm,
Thanks for the fast reply. Yes, sorry i was not clear. I am talking about the discovery board. Right now there are no changes in the hardware, i just have the board and an usb cable to flash images. As the pre-compiled code from the bin directory works fine and both IDEs are based on the same compiler and similar configuration scripts, i was expecting that would be easy to convert. For my final project i would use probably TLV320AIC23B, this is why i didn't dig deep into the pdf of the chip soldered on the discovery board yet. Yeah, i have a scope and a good logic analyzer also, right now i believe i miss some compiler define or something, even i searched into all Attolic files and believe all is done as it should be. Regards2012-10-17 10:11 AM
All fixed now.
For future reference, if somebody need this. After reading this topic: http://www.coocox.org/forum/topic.php?id=756&page=4 The post from . It seems one of the CoCox file is wrong/incomplete/whatever: so the Audio_playback_and_record\src\system_stm32f4xx.c needs to be inserted in the CoIDE project instead of the automatically added one. BRWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.