2018-11-15 12:54 PM
Hi to All !
I'm a new in STM32 MCU programming. (But with big experience in C/C++).
Just bought STM32L4R9I-DISCO, install eclipse with plugin for AC6 toolchain, STM32Cube under Linux. Build one of the examples : RTC-timestamp, erase the Flash (without problems) and try to install example, but got :
=========================================================
auto erase enabled
Info : Device id = 0x10036470
Info : STM32L4xx flash size is 2048kb, base address is 0x8000000
Info : Erase the padded zone before the write
Error: Whole bank access must start at beginning of bank.
target halted due to breakpoint, current mode: Thread
xPSR: 0x61000000 pc: 0x20000050 msp: 0xfffffffc
Info : block write succeeded
wrote 16384 bytes from file Debug/STM32L4R9I-Discovery_RTC_TimeStamp.elf in 0.443163s (36.104 KiB/s)
** Programming Finished **
** Verify Started **
target halted due to breakpoint, current mode: Thread
xPSR: 0x61000000 pc: 0x2000002e msp: 0xfffffffc
target halted due to breakpoint, current mode: Thread
xPSR: 0x61000000 pc: 0x2000002e msp: 0xfffffffc
verified 16112 bytes in 0.506380s (31.072 KiB/s)
** Verified OK **
shutdown command invoked
===================================================
in my ...FLASH.ld :
===================================================
/* Specify the memory areas */
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 640K
FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 1024K
}
===================================================
What is my mistake ? I not changed example package in any way ...
***********************************************************
My second question : Can I restore factory image with demonstration on the LCD ?
Sorry, if my questions seem to you too stupid, but excuse my first attempts with STM32 programming !
Thank you for you help in advance !
Regards,
Branimir
Solved! Go to Solution.
2018-11-15 1:21 PM
The L4R may have different flash banking options that the OpenOCD software is not entirely capable of dealing with.
Unless you saved the original content perhaps not exactly
There are some .HEX files in the various demo directories for CubeL4
STM32Cube_FW_L4_V1.13.0\Projects\32L4R9IDISCOVERY\Demonstrations\STemWin\Binary\STemWin-STM32L4R9I-Discovery_V1.0.0.hex
These might require the ST-LINK Utilities, and its External Loaders
2018-11-15 1:21 PM
The L4R may have different flash banking options that the OpenOCD software is not entirely capable of dealing with.
Unless you saved the original content perhaps not exactly
There are some .HEX files in the various demo directories for CubeL4
STM32Cube_FW_L4_V1.13.0\Projects\32L4R9IDISCOVERY\Demonstrations\STemWin\Binary\STemWin-STM32L4R9I-Discovery_V1.0.0.hex
These might require the ST-LINK Utilities, and its External Loaders
2018-11-15 2:06 PM
Later, I found, that no matter of this error program is flashed on target ;)
Thank you for your answer !
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.