2024-05-27 7:21 AM - last edited on 2024-05-27 9:05 AM by Tesla DeLorean
Hi I m using F072 Nucleo bd, and compiler report the following errors but there was no syntax error from the code, can anyone advise?
22:08:09 **** Incremental Build of configuration Debug for project F072_GPS_ NEO-6M_i2c_LCD_16x2 ****
make -j8 all
arm-none-eabi-gcc -o "F072_GPS_ NEO-6M_i2c_LCD_16x2.elf" @"objects.list" -mcpu=cortex-m0 -T"C:\Users\user\Documents\________STM32\F072_GPS_ NEO-6M_i2c_LCD_16x2\STM32F072RBTX_FLASH.ld" --specs=nosys.specs -Wl,-Map="F072_GPS_ NEO-6M_i2c_LCD_16x2.map" -Wl,--gc-sections -static -u _printf_float --specs=nano.specs -mfloat-abi=soft -mthumb -Wl,--start-group -lc -lm -Wl,--end-group
c:\st\stm32cubeide_1.9.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.0.202111181127\tools\arm-none-eabi\bin\ld.exe: ./Core/Src/uartRingBuffer.o:C:/Users/user/Documents/________STM32/F072_GPS_ NEO-6M_i2c_LCD_16x2/Debug/../Core/Src/uartRingBuffer.c:15: multiple definition of `huart1'; ./Core/Src/main.o:C:/Users/user/Documents/________STM32/F072_GPS_ NEO-6M_i2c_LCD_16x2/Debug/../Core/Src/main.c:49: first defined here
collect2.exe: error: ld returned 1 exit status
make: *** [makefile:64: F072_GPS_ NEO-6M_i2c_LCD_16x2.elf] Error 1
"make -j8 all" terminated with exit code 2. Build might be incomplete.
22:08:09 Build Failed. 2 errors, 0 warnings. (took 506ms)
2024-05-27 9:08 AM
It's not a syntax error, and it's not from the compiler.
The LINKER is complaining that you define things in multiple places, so
a) Don't understand how to use include/ source files properly
b) Don't understand how to use extern properly
Put the definition of a variable in ONE place, in a C source file. Put prototype for global variables in an include file with an extern property so the global can be accessed across multiple source files.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.