2011-10-30 12:01 AM
Hello,
I have STM3210C-EVAL board. The HID mouse example is working well.But, if I change the endpoint from 0x81 to 0x82, it doesn't work.In addition, for TX2 buffer I changed buffer size to 128 like#define TX2_FIFO_FS_SIZE 128.Andybody with this kinds of problem?2013-10-22 12:38 AM
can answer me if you resolve the problem ?
how you resolve the problem?2013-10-22 5:11 AM
A single post from two years ago, probably not.
Please state clearly your situation and perhaps you can get an answer about that.2013-10-22 10:01 AM
My guess is that you should increase by one value of
#define EP_NUM located in usb_conf.hWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.