2008-02-18 12:45 AM
Encoder Mode
2011-05-17 3:23 AM
Hi STOne-32 / All.
I wish to use the Encoder Mode (a sub mode of the TIMers). This uses two signals in quadrature to count from an incremental encoder. -------------------------------------------------------------------------- Q1 : Is there any example code for this mode? -------------------------------------------------------------------------- Q2 : Is it possible to cascade two timers in encoder mode - to get 32 bit counting? (I'm guessing not because you'd need two trigger out lines from the master and two trigger in lines for the slave. There only seems to be 1 trigger available). Note: I've read the post about ''Cascading timers overflow handling and capture'' by andywild (Posted 20-01-2008 at 12:29) and AN2592 in detail. -------------------------------------------------------------------------- Q3 : To Use Encoder Mode, do I have to use TIMx_CH1 & TIMx_CH2 pins (or can I use any e.g. TIMx_CH3 & TIMx_CH4) -------------------------------------------------------------------------- Please could you give me some advice! Thanks.2011-05-17 3:23 AM
Hi All,
Any ideas on using the Timers in Encoder Mode (as per my first query)? ThanxWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.