2018-03-25 10:10 PM
I am using STPM32 with STM32F4 microcontroller series. We are using UART communication. When we trying to reset the whole framework the controller only receives 0 values for 48th register. When we are trying to set the dsp_reg3 register also, stpm returns 0 value. But when we use evaluation software to reset the device it is working fine. Is there anything missing while setting up UART.?
2018-05-03 8:24 AM
Hi, i am an embedded electronic engineer and lately i have a project named 'plug meter' based on an STM32 MCU and the STPM01 AFE, but i couldn't establish the SPI communication between AFE and MCU because there are no libraries to read and write through SPI that are compatible with the STPM01, please help me!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.