2023-06-22 2:07 PM - last edited on 2023-07-12 2:43 AM by Amel NASRI
Hi,
I would like to test the EMW3080 with the STM32H5, as I understand it is necessary to load the firmware provided by the ST in order for the EMW3080 to work with the driver provided for the B-U585I-IOT02A board. Correct?
Does ST have plans to launch any H5 kit with wifi, preferably using a wifi module with better support and availability, like the new nRF7002 and CC3301?
2023-07-12 5:47 AM
Hello @AMend.7 ,
The MXCHIP EMW3080B firmware programmer is for the B-U585I-IOT02A board.
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-09-08 5:44 AM
The WiFi firmware update for STM32H573I-DK + MB1400 daughter board with MXCHIP EMW3080B is also available at https://www.st.com/en/development-tools/x-wifi-emw3080b.html with the V1.1.0.
Some Wi-Fi examples for this board can be found under STM32Cube_FW_H5_V1.1.1\Projects\STM32H573I-DK\Applications\NetXDuo\...
The Wi-Fi examples are the ones with the _wifi suffix.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.