2018-01-08 10:07 PM
We are designing for an application having front and back-facing 7' displays. I am keen to hear suggestions for running both displays from the same processor using using LTDC or display peripheral?
Both displays will have different images.
Resolution will be somewhere around 800 x 480 in each display, so relatively lo-res.
2018-01-16 5:32 PM
That's a much better solution.
no CPU overhead to refresh the screen, its a huge difference in performance.
as many displays as you want. with a fast update.
otherwise, SPI is the best but the update speed is like 1000x slower than the 'MCU interface.'
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.