2023-01-23 8:06 AM
Hi,
I want to compute the moving average of an IR sensor and set the brightness of an LED and im taking input values from read and I have set up an a timer interrupt which gets triggered every 100ms, and with this trigger I'm saving the read values into an array of size 10. My window size is 10. When I'm running the values keep running very rapidly to infinity. Please help. Thank you. Please check the timer interrupt loop for moving average, I feel something is wrong there.
uint16_t read;
float MA[10];
float sum =0;
uint16_t i=0;
uint16_t j=0;
while (1)
{
/* USER CODE END WHILE */
HAL_ADC_Start(&hadc1);
HAL_ADC_PollForConversion(&hadc1, 100);
read = HAL_ADC_GetValue(&hadc1);
if(sum >=2470 && sum <=2530){
__HAL_TIM_SET_COMPARE(&htim2, TIM_CHANNEL_1, 1000);
}
else if(sum>=999 && sum <=2470){
__HAL_TIM_SET_COMPARE(&htim2, TIM_CHANNEL_1, sum/5);
}
else if(sum >= 2530 && sum <=4095){
__HAL_TIM_SET_COMPARE(&htim2, TIM_CHANNEL_1, (5095-sum)/5);}
}
}
}
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim){
float window_size = 10;
if(htim->Instance == TIM3){
MA[i%10] = read;
i=i+1;
for(j=0;j<10;j++){
sum = sum + MA[j]/window_size;
}
}
}
Solved! Go to Solution.
2023-01-23 2:09 PM
You forgot to set the sum to 0 before computing the running average.
2023-01-23 10:08 AM
ADC sample can get triggered by a signal, which can be a pin.
A PWM can be generated by a TIMER and output to a pin.
Connect both pins with a wire.
now the PWM period must be longer than the ADC sample time (here time scale is far from the limits)
The DMA can store the ADC measured sample in a buffer (10 16-bit values), which can be written in cyclic mode. At any time you select, read the 10 samples and make the average. This should be the moving average.
There are many other ways to do it. This to me is HW assisted, works when cranked up in speed.
2023-01-23 2:09 PM
You forgot to set the sum to 0 before computing the running average.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.