2017-12-30 9:13 AM
Hello,
is someone using a STM32L496ZG Nucleo-144 Board? I tried to set up a blinky LED via LL_hal functions, as well as an USART. But without any result. The led is still off and the usart doesnt work.
When I set each bit on my own, the led blinks. (To do this with uart gives me a lot of compiler errors. See my other post. So I cant test this currently).
When I try the same (blinky LED and USART) with a STM32F072 Nucleo-64 board, everythink works find, including to receive values in my terminal via USART.
Is my Nucleo-144 defect or doesnt the lib work correct? Does someone hase any experience?
What can I do, if my board is defekt (which is kindly new..)?
Kind regards
#stm32l496zgWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.