2018-02-06 11:32 PM
Hi, I want to do a confirm that does STM32F103RC support UVC(USB video class)? Because I don't find the UVC related driver in STM32Cube_FW_F1_V1.6.0\Middlewares\ST\STM32_USB_Device_Library. We want to use camera is UVC and driver IC is TUSB1210. Can
S
TM32F103RC
support this?2018-02-08 2:05 AM
The MCU supports it as any other class because it is just a software layer that uses some endpoints. However it only supports Full Speed mode (12Mbps), which may not be feasible for video streaming.
2018-02-08 8:20 AM
I don't recall the F1 series supporting ULPI PHY's
UVC is not something ST has historically provided examples for, you'll likely need to own the development task, or find a vendor providing more expansive USB stack libraries. Discuss with the local ST Rep/FAE supporting your project/company.
The F1 is an Old device, there are surely better STM32 solutions in 2018?
2018-02-10 10:07 PM
Do mcu must have ULPI PHY?
2018-02-10 11:33 PM
1. Still picture is OK for UVC. Right?
2. Does the MCU need
ULPI PHY
?2018-02-13 10:25 AM
1. A still picture would be better interfaced with Mass Storage Class, or Picture Transfer Protocol.
2. All USB peripherals in STM32 line have Full Speed PHY embedded in the MCU, and since this isn't a High Speed capable device, ULPI cannot be used.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.