2022-05-16 3:11 AM
That's how I would understand it. When I set the output as open drain I need an external pull-up (or pull-down) resistor. Is there a reason I SHOULD use the external resistor? If so - what does this configuration option (pull-up, pull-down) mean exactly?
2022-05-16 5:17 AM
2022-05-16 7:02 AM
@Adam �?yskawa "Is there a reason I SHOULD use the external resistor?"
Anytime that the internal pullup is not suitable for your application; eg, its resistance is too high.
As the document linked by @Pavel A. says, the typical internal pullup value is ~ 40k - so that's going to be too much for typical I2C.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.