2022-07-28 7:50 PM
hi,
i'm porting of little file system in to the m7 b/d
after the porting task is done, it can not be operated properly.
it prints to the console 'corrupted dir pair at 0x0 0x1'
i don't know why this print message..
here is my lfs settings
#define LFS_READ_SIZE 32
#define LFS_PROG_SIZE 32
#define LFS_STM32F7_GRAN 2048
#define LFS_BLOCK_CNT 4
#define LFS_CACHE_SIZE 512
#define LFS_LOOKAHEAD_SIZE 512
#define LFS_BLOCK_CYCLES 500
// configuration of the filesystem is provided by this struct
const struct lfs_config cfg = {
.context = "stm32f746",
// block device operations
.read = hal_block_device_read,
.prog = hal_block_device_prog,
.erase = hal_block_device_erase,
.sync = hal_block_device_sync,
// block device configuration
.read_size = LFS_READ_SIZE,
.prog_size = LFS_PROG_SIZE,
.block_size = LFS_STM32F7_GRAN,
.block_count = LFS_BLOCK_CNT,
.cache_size = LFS_CACHE_SIZE,
.lookahead_size = LFS_CACHE_SIZE,
.block_cycles = LFS_BLOCK_CYCLES,
};
any feedback plz..
thanks
2022-07-29 7:45 AM
Here you can find a helping hand for your project.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.