2020-12-08 7:13 AM
I'm looking to use this controller for aerospace applications and was wondering if there was any performance data at the -55`C temperature extreme. A required warm-up period or something similar is what I'm expecting to need, but any more detailed information would be helpful.
Solved! Go to Solution.
2020-12-08 8:19 AM
The STM32 are guaranteed to work in the temperature range given in the datasheet and by the order number, while the lowest temperatur is always -40 DEGC.
The particular datasheet also lists the storage temperature range, which is for the STM32L432: -65...150 DEGC.
Does it answer your question?
Regards
/Peter
2020-12-08 8:19 AM
The STM32 are guaranteed to work in the temperature range given in the datasheet and by the order number, while the lowest temperatur is always -40 DEGC.
The particular datasheet also lists the storage temperature range, which is for the STM32L432: -65...150 DEGC.
Does it answer your question?
Regards
/Peter
2020-12-08 8:39 AM
Hey Peter,
I'm really looking for information on whether the STM32 is functional, at all, down to -55`C. I fully understand that functionality is not guaranteed at that temperature. The application we're evaluating these parts for will require testing at this low temperature. The STM32 would be inside a housing that will get warmer than ambient, but on start-up the chip would be subject to that temperature. I'm looking to see if there's any data that you might have to indicate what performance could be expected and whether a warm-up period would be required to achieve partial or full functionality.
Thank you for your help!
2020-12-08 8:55 AM
At that temperature, a lot can happen. Often ceramic capacitors (Z, Y, Z ceramics loose temperature. What about having some mechanical temperature switch, heating up to -40 and only then starting the electronic?
2020-12-08 9:16 AM
If operating at -55 C is critical to your application, I would never use a part which is only specced to -40C. Even if you fully test it, there is no guarantee that it will work in future production batches of chips. Aerospace applications tend to be lower quantity and higher cost--find a more appropriate chip.
2021-01-04 5:41 PM
While -55 C may seem cold to some, there are the brave overclockers with liquid nitrogen.
Overclocking to 7GHz with Liquid Nitrogen Hands-On Computex 2017
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.